January 2018
Solution Highlights  
MJPEG on Minized + TDNext camera

This design offers complete video pipeline system implementation with motion JPEG compression engine as well as wireless video transmission over Wifi. This embedded vision development platform makes it easy to adopt Xilinx Zynq family of ARM plus FPGA Accelerated video processing platform at a low cost. Developing differentiated smart surveillance, video analytics and deep learning end products is also a breeze.
• Frame rate : 25 fps@1920x1080
• Platform Linux OS runs web server and MJPEG streaming
  service
Contents
MJPEG on Minized + TDNext camera
News Update
Featured Product
Resources
News Update
IAS Industrial Automation Show, 7-11 November 2017, Shanghai
At the recent IAS in Shanghai, Xilinx presented the following eight solutions centering on the key theme of “Xilinx Makes Factories Smarter”. As Xilinx’s global strategic partner, Avnet was onsite to demonstrate and explain about the ZYNQ-based motor control and vision/infrared sensor fusion solutions which attracted many visitors to the booth.
 • reVISION pedestrian detection  • Motor control
 • Intelligent logistics  • Sensor fusion
 • POWERLINK open automation  • EtherCAT/RTEX controller
 • Robot vision positioning  • Multi-axis motion control and drives
Avnet MiniZed Speedway
Avnet announced that registration is now open for a series of interactive SpeedWay Design Workshops™ to help engineers jump-start the development of single-core Xilinx® Zynq®-7000 All Programmable SoC devices using the Avnet MiniZed™ Zynq SoC development kit, a cost-optimized prototyping platform for embedded vision and Industrial IoT systems. These one-day instructional programs, hosted by Avnet in more than 40 cities across North America, Europe and Asia, will train customers on the latest design flows using Xilinx’s Vivado®Design Suite through a mix of lecture and interactive labs. This Speedway in Asia plan to be launched in Q1 2018.
News Update Avnet MiniZed: Zynq single-core development kit shipping now
MiniZed™ is a Zynq 7Z007S single-core development board.
News Update Arty S7-50: Xilinx Spartan-7 development kit shipping now
Spartan-7 FPGA Board with 1 MSPS On-Chip ADC for Makers and Hobbyists USB-UART Bridge
News Update Avnet UltraZed-EG: ZU3EG with production ZU3EG device shipping now
The UltraZed-EG Starter Kit consists of the UltraZed-EG System-on-Module (SOM) and IO Carrier Card bundled.
News Update Spartan-6 product shipments to at least 2027, ISE supported on WIN10
Spartan®-6 devices offer industry-leading connectivity features.
Featured Products
Feature Product UltraZed-EV starter kit
The UltraZed-EV™ Starter Kit consists of the UltraZed-EV System-on-Module(SOM) and Carrier Card bundled to provide a complete system.
Feature Product UltraZed PCIe Carrier Card
Supports the UltraZed-EG™ System-on-Module (SOM), providing easy access to the full 180 user I/O, 26 PS MIO, and 4 PS GTR transceivers available from the UltraZed-EG SOM.
Feature Product Xilinx Virtex UltraScale+ FPGA VCU1525 Acceleration Development Kit
Ideal for data center application developers wanting to leverage the advanced capabilities of Virtex® UltraScale+™ FPGAs.
Resources
▶ Key Attributes of an Intelligent IIoT Edge Platform
▶ Xilinx Developer Forum materials available now
▶ Webinar: Use ZCU102 TRD to Accelerate Development of ZYNQ UltraScale+ MPSoC (Chinese)
Quick Links
Xilinx product
and solution Guide
►

Automotive
Solution Guide
►

Design
Resource Center
►
Contact ► Buy ►

© 2018 Avnet, Inc. All rights reserved.
The Avnet Inc. logo and Reach Further are trademarks of Avnet, Inc. All other products, brands and names are trademarks or registered trademarks of their respective owners.
This email was sent by: Avnet Asia, 151 Lorong Chuan, New Tech Park, #06-03, Singapore 556741
Unsubscribe


If you prefer not to receive Avnet updates in future, please unsubscribe here.