Avnet Asia Connect
 
 
ON Semiconductor - CMOS 图像传感器



Onsemi公司是CMOS影像解决方案的全球性供应商,其不断扩大的产品组合被用于所有领先的行动电话和笔记型电脑品牌。 Onsemi还提供范围广泛的产品,用于数位相机和摄影机、监控、医疗、汽车和工业应用、视讯会议、条码扫描器、玩具和游戏。 Onsemi致力于为各种应用场合提供影像支援(Imaging Everywhere™),不断推动市场创新,如推出用于傻瓜混合式相机(MT9F001)的首款14MP CMOS影像感测器,以及业界首款¼英寸格式的5MP SOC(MT9P111)。

在网络高清监控摄像机方案中,Onsemi公司的AR0130和AR0230 CMOS图像传感器被业内多家摄像机制造商所采用,并广泛应用于130万和200万网络摄像机中


全球汽车市场图像传感器的领袖,占所有汽车传感器第一位,份额50%,ADAS市场第一位,份额70%
• 2004年推出世界首款汽车CMOS图像传感器
• 推出世界首款汽车功能安全完整性等级(ASIL)图像传感器
• 同类最佳的全局快门,可以用于车舱内乘客监控,疲劳驾驶监测
• 注于汽车品质标准AECQ100 质量认证,个位数PPM质量保证






特色

• Leader of the global auto market image sensor
• These are all for the first car sensor, share 50%. These are the first ADAS market share of 70%.
• the launch of the world's first car CMOS image sensor in 2004
• note to automobile quality standards
• These are AECQ100 quality certification. These are a number of PPM quality assurance
• The best global shutter of the same kind can be used .These car passenger cabin monitoring.
• These are the fatigue driving monitoring



应用

• Auto: Advanced Driver Assistance Systems (ADAS), Automotive Viewing, Emerging Automotive Applications
• Industrial: Machine Vision, Intelligent Transportation Systems, Medical, Scientific, High-end Surveillance
• Consumer: Mobile, Sports Cam, PC / Gaming, Security / Surveillance, Other Consumer



方块图





Learn More







▲回頁首
 
avnet.com/apac  
Copyright ©2018 Avnet, Inc. All rights reserved.