Avnet Asia Connect
 
 
ON Semiconductor - CMOS圖像感測器



ON Semiconductor 公司是CMOS影像解決方案的全球性供應商,其不斷擴大的產品組合被用於所有領先的行動電話和筆記型電腦品牌。 Onsemi還提供範圍廣泛的產品,用於數位相機和攝影機、監控、醫療、汽車和工業應用、視訊會議、條碼掃描器、玩具和遊戲。 Onsemi致力於為各種應用場合提供影像支援(Imaging Everywhere™),不斷推動市場創新,如推出用於傻瓜混合式相機( MT9F001)的首款14MP CMOS影像感測器,以及業界首款¼英寸格式的5MP SOC(MT9P111)。

在網絡高清監控攝像機方案中,Onsemi公司的AR0130和AR0230 CMOS圖像感測器被業內多家攝像機​​製造商所採用,並廣泛應用於130萬和200萬網絡攝像機中
。

全球汽車市場圖像感測器的領袖,佔所有汽車感測器第一位,份額50%,ADAS市場第一位,份額70%
• 2004年推出世界首款汽車CMOS圖像感測器
• 推出世界首款汽車功能安全完整性等級(ASIL)圖像感測器
• 同類最佳的全局快門,可以用於車艙內乘客監控,疲勞駕駛監測
• 注於汽車品質標準 AECQ100 質量認證,個位數PPM質量保證






特色

• Leader of the global auto market image sensor
• These are all for the first car sensor, share 50%. These are the first ADAS market share of 70%.
• the launch of the world's first car CMOS image sensor in 2004
• note to automobile quality standards
• These are AECQ100 quality certification. These are a number of PPM quality assurance
• The best global shutter of the same kind can be used .These car passenger cabin monitoring.
• These are the fatigue driving monitoring



應用

• Auto: Advanced Driver Assistance Systems (ADAS), Automotive Viewing, Emerging Automotive Applications
• Industrial: Machine Vision, Intelligent Transportation Systems, Medical, Scientific, High-end Surveillance
• Consumer: Mobile, Sports Cam, PC / Gaming, Security / Surveillance, Other Consumer



方塊圖





Learn More







▲回頁首
 
avnet.com/apac  
Copyright ©2018 Avnet, Inc. All rights reserved.