Avnet Asia Connect
 
 
Venturing Further in LORA





The advent of LoRa has been hailed as a major advancement in wireless technology. By enabling long distance low data rate communication of sensors and actuators, it has fuelled vast developments in M2M and IoT, and created unprecedented opportunities for engineers to innovate.

As the pre-eminent leader in the technology field, Avnet has devised the LoRa Node Evaluation Kit to be an indispensable tool that innovators rely on to spearhead new designs. Based on the Semtech SX1272 LoRa transceiver, and the STM32L072KB low-cost low-power 32-pin package entry level Cortex M0+ MCU, the kit is the culmination of our deep expertise and relentless drive to accelerate connectivity designs that stand up to market expectations.




Features

• Supports 920 or 868 MHz band
• Meets LoRaWAN specification
• LoRa node platform targeted for broad-based IoT application
• Demo on Actility Thingpark wireless platform



Key Components

• SX1272/SX1276 - Semtech
• STM32L071 - STM
• B39921B3407U410 - Epcos



Target Applications

• Metering (water, gas and energy)
• Sensor node
• GPS tracking
• Wearables




Block Diagram








▲TOP
 
avnet.com/apac  
Copyright ©2017 Avnet, Inc. All rights reserved.