Avnet Asia Connect
 
 
Making the leap into everyday life





EVEN IN ANCIENT TIMES, PEOPLE HAD A VISION OF MACHINES THAT WOULD AUTONOMOUSLY HELP THEM IN THEIR DAY-TO-DAY LIVES. TODAY, THE SCIENCE OF ROBOTICS IS ABOUT TO MAKE THE LEAP FROM INDUSTRY INTO EVERY AREA OF HUMAN LIFE, SO REALISING THAT AGE-OLD DREAM.

The ancient Greek scientist and philosopher Aristoteles wrote in his work “Politics”: “If every tool could perform its own work when ordered, or by seeing what to do in advance ... master-craftsmen would have no need of assistants and masters no need of slaves.” The subsequent centuries have seen the invention of machines with sometimes quite astounding capabilities. Such advances came to a first fruition in the 18th century. In 1740, for example, Jacques de Vaucanson created an automated duck capable of flapping its wings and drinking water. He also developed the first fully automatic weaving loom.



THE ORIGINS OF THE WORD “ROBOT”

The word “robot” was not coined until the 20th century – in a theatre play, “Rossum’s Universal Robots”, published in 1920 by Czech author Karel Čapek. The drama is about artificial humans – robots – who serve as cheap labour, devoid of all rights, and ultimately rebel against their human masters. It was not until the 1940s that the word “robot” really became widespread, however, through the writings of science-fiction author Isaac Asimov. Initially used only to describe human-like machines, the word “robot” today covers a wide range of different machinery. In fact, it is still not unambiguously defined even today. A sound basis for judging when a machine can be described as a robot is provided by the Robotic Industries Association: “A robot is a programmable, multifunction manipulator designed to move material, parts, tools, or specific devices through variable programmed motions for the performance of a variety of tasks.”


FIRST USE OF ROBOTS IN THE AUTOMOTIVE INDUSTRY

The first robot meeting the above criteria was patented in the USA in 1954. Georg Devol developed a programmable manipulator named “Unimate” for gripping and moving components. After having tried to market his invention for almost 10 years, he sold the patent to Joseph F. Engelberger. The engineer and businessman modified the robot, and his company Unimation finally succeeded in bringing it to market, selling 8,500 of the machines in total. And so it is that Engelberger is regarded as “the father of robotic”. The numbers of robots employed in factories have been steadily rising ever since. They peaked in 2015, with some 1.6 million robots in use worldwide. According to the International Federation of Robotics (IFR), that figure is forecast to rise to 2.6 million by 2019.


FROM AN INDUSTRIAL WORKER TO A PARTNER IN EVERYDAY LIFE

The rapid advances in sensor and microprocessor technology in recent years have steadily expanded the robots’ range of abilities. Nowadays they are able to detect objects, navigate autonomously, sensitively handle objects with their grippers, and move freely even around difficult terrain. “After some 50 years of robot use in industry – primarily in automobile manufacture – we are about to see them make the leap into wider areas of society,” asserts Professor Ingrid Ott from the Karlsruhe Institute of Technology. “There have been major technical advances in robotics in the recent past. As a result, robots are not only becoming ever smaller, lighter, cheaper and more flexible to use, they are also increasingly moving out of the secure areas of industrial mass production and working directly alongside human beings.” So-called service robots – assisting in clinical care, handling logistics, or cleaning business premises and private households – will “in just a few years attain higher global market volumes than classic industrial robots. A number of global corporations are investing huge resources researching robot assistance systems for all areas of life.” The robots of the future will not only be strong, fast and precise; they will also help humans as efficient, communicative partners in their day-to-day existence.


ROBOTS LEARNING TO FEEL

According to Professor Dr Martin Venhaus, Head of the robotics, image processing, computer-aided data processing and sensor technology labs at the Sudwestfalen university of applied sciences, robot technology is also being increasingly integrated into other products. “I am seeing the dividing line steadily disappear. A good example is automated driving,” Venhaus reports. The university is looking to work on the voice and gesture recognition capabilities of robots in future. 3D imaging and smartphone interfacing will also be subjects for research. “And not least, we want to teach our robots to feel, enabling even closer human-machine interaction,” says Venhaus. To that end, robots will in future increasingly be equipped with artificial intelligence. That will mean they will be able to recognise and interpret human emotions, and also make their own decisions. Then robots will be capable of working truly autonomously, with no human intervention – and the vision of Aristoteles will have become reality.







▲TOP
 
avnet.com/apac  
Copyright ©2017 Avnet, Inc. All rights reserved.