GPUTOP(8)
Marius Vlad marius-cristian.vlad@nxp.com
October 25, 2018



NAME


GPUTOP -- Monitor GPU clients memory, hardware counters, occupancy state
load on DMA engines, video memory and and DDR memory bandwidth (only
under Linux).



SYNOPSIS


GPUTOP [options]

GPUTOP -m [mode] -- Where mode can be: MEM, COUNTER_1, COUNTER_2,
OCCUPANCY, DMA, VIDMEM and DDR (under Linux/Android). Use this option to
start GPUTOP directly in a mode that you're interested on. For COUNTER_1
and COUNTER_2 a context will be needed. See _NOTES_ section why this is
necessary.

GPUTOP -c ctx_no -- specify a context to attach when display
context-aware hardware counters.

GPUTOP -b -- display in batch mode. For other modes than memory, this
will only take an instantaneous sample. See -f

GPUTOP -f -- Use this when using GPUTOP from a script.

GPUTOP -x -- useful to display contexts when used with ``-b''

GPUTOP -i -- ignore warnings about kernel mismatch

GPUTOP -h -- display usage and help


Interactive mode

Normally, when starting up, GPUTOP, starts in interactive mode. The
following are a list of useful commands:

-   'h' -- display help page
-   '0-6'/Left-Right arrows -- switch between viewing pages
-   'x' -- display application contexts
-   'SPACE' -- select a context that you want to track. Useful for
    reading COUNTER_1 and COUNTER_2 values.
-   'r' -- useful for hardware-counter pages to display different
    viewing modes (switches between different modes of
    aggregation: MIN/MAX/AVERAGE/TIME)
-   'q'/ESC -- exits GPUTOP.
-   'p' -- stops reading counter values and displays only
    current values. Useful to get a instantaneous values of
    the counters.



DESCRIPTION


GPUTOP can be used to determine the memory usage your application is
using, or to read the hardware counters exposed by the GPU in real-time.
Additionally, DMA engines and Occupancy states are displayed. GPUTOP has
multiple viewing pages: a MEMORY USAGE page, two HARDWARE COUNTER pages,
a DMA ENGINE page and an OCCUPANCY page. When normally started, GPUTOP
will be in interactive mode. Type 'h' to get a list of the current
keybindings.



REQUIREMENTS


Linux

GPUTOP requires access to DEBUGFS sub-system on Linux in order to
display memory usage, used by clients submitting commands to the GPU.
GPUTOP will try to mount the DEBUGFS pseudo-filesystem if it is not
already mounted. In order to read hardware counters the profiler must be
activated in the driver. Usually this can be set by loading the driver
with GPUPROFILER=1 POWERMANAGEMENT=0 options, or by adding a line to
/ETC/MODPROBE.D/GALCORE.CONF with those parameters. See you distro
manual on how to to do that.

QNX

Just like in Linux, in order to be able to read the hardware counter
values GPU-GPUPROFILER has to be set to 1 in
graphics.conf'' file under $GRAPHICS_ROOT directory. Other views likeoccupancy''
and DMA will require GPU-POWERMANAGEMENT to be set to 0 (disabled).



NOTES


Sampling hardware-counters

GPUTOP samples the driver for hardware counter values. Internally the
driver will update the values of the counters whenever the application
submits a special type of command to the GPU. Depending on how fast that
happens GPUTOP can't foresee/adjust the values of the counters. So
tweaking the amount of sample taken or the delay time doesn't really
help. For dealing with situations where the application will submit
either to fast or to low commands to the GPU, several modes of viewing
counters has been added. Cycle between them to understand or get a
bird-eye view of the counter values. Empirically MAX/AVERAGE displays
the closes values to the truth.


Context-aware counters

COUNTER_1 and COUNTER_2 are context-aware counters (i.e.: tied to an
application).

Internally the driver assigns various context IDs to the application
submitting commands to the GPU. These contexts IDs are currently
required to read those hardware counter values. Either use -X on the
command line (together with -B option and choosing -M MEM viewing mode),
or for interactive mode use 'x' and then 'SPACE' to show and select a
context ID.

In case you are getting zero'ed out values for COUNTER_1 and/or
COUNTER_2 values, cycle thru the available counter IDs.

Due to the way the driver is built, for single-GPU core applications
will have TWO context-ids. Empirically the largest integer values holds
the real context-id.


Unsupported GPUs

Do note, that on newer GPU cores, like GC7000 models, the behaviour is
different and it is not ONLY SUPPORTED in driver version newer than
6.2.4p1 (Build at least 150331).

For GCV600 (i.MX7ULP and i.MX8MM) the IDLE/LOAD register is not
available hence GPUTOP will display incorrect (inversed) values.



PAGES


Client attached page

When viewing client attached page the following head columns are
displayed:

PID RES(kB) CONT(kB) VIRT(kB) Non-PGD(kB) Total(kB) CMD

-   PID -- process id
-   RES -- reserved memory
-   CONT -- contiguous memory
-   VIRT -- virtual memory
-   Non-PGD -- Non-paged memory
-   Total -- the sum of all above
-   CMD -- the name of the application (trimmed)

These memory items correspond to memory pools in the driver.


Vidmem page

When viewing vidmem page the following head columns are displayed for
each process.

PID IN VE TE RT DE BM TS IM MA SC HZ IC TD FE TFB

-   IN -- index
-   VE -- vertex
-   TE -- texture
-   RT -- render target
-   DE -- depth
-   BM -- bitmap
-   TS -- tile status
-   IM -- image
-   MA -- mask
-   SC -- scissor
-   HZ -- hz
-   IC -- i_cache
-   TD -- tx_desc
-   FE -- fence
-   TFB -- tfb header



EXAMPLES


When using ``-b'' option GPUTOP will start in interactive mode and
execute just once its main loop. This is useful for various reason,
either to get an instantaneous view of a different viewing page, or
scripting.

-   Get a list of processes attached to the GPU

    $ gputop -m mem -b

-   Get a list of processes attached to the GPU, but also display the
    contexts ids

    $ gputop -m mem -bx

-   Display counters (counter_1) using context_id

    $ gputop -m counter_1 -b -c

-   Display counters (counter_2) using context_id

    $ gputop -m counter_2 -b -c

-   Get IDLE/USAGE

    $ gputop -m occupancy -b | grep IDLE



SEE ALSO


-   under QNX see GRAPHICS.CONF for disabling powerManagement and
    enabling gpuProfiler.
-   under Linux see /SYS/MODULES/GALCORE/PARAMENTERS/GPUPROFILER and
    /SYS/MODULES/GALCORE/PARAMETERS/POWERMANAGEMENT.
-   _libgpuperfcnt(8)_